Sustainability Eco Cable
Eco Cable
ECO CABLE, green inside
We provide products that are the green life blood that brings energy and communications to homes, infrastructures and cities around the world.
With a business strategy consistent with the UN Sustainable Development Goals, we strive to be green inside.
We express this through products that when installed in homes, infrastructures and cities around the world, make these just as green inside. ECO CABLE is the first green label in the cable industry and vouches for the greenness of our cables.
Prysmian Group ECO CABLE, Green Inside
Six measurable and known criteria
To be ECO CABLE-labelled, each cable family has to pass a rating process based on the following criteria:
Carbon Footprint
Calculated according to “cradle-to-gate” approach and combined with other parameters to achieve full “cradle-to-grave” carbon footprint.
Substances of Very High Concern
Absence of substances that are carcinogenic, mutagenic, toxic for reproduction, or hazardous for the environment.
Recyclability/Circularity
Materials used in cables are potentially recyclable or products themselves are potentially fully recyclable.
Recycling Input Rate
Presence of recycled material in a cable, both purchased from external suppliers and reused by Prysmian Group itself.
Environmental Benefits
Low-carbon enabling products, CPR compliant cables and cables used for green energy sources.
Cable Transmission Efficiency
The more efficient the cable, the more sustainable its performance. For Optical cables this means an increase in fibre density.
Carbon Footprint, Reciclability/Circularuty, Recycling Input Rate
Environmental Benefits, Cable Transmission Efficiency
Substances of Very High Concern
Our Target
ECO CABLE is our pledge to provide transparent and clear indications and information, using recognized criteria, on the greenness of our cables based on our three key drivers: SUSTAINABILITY, RELIABILITY and QUALITY.